Is it possible to implement secure boot without using trust zone for stm32U585??
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-24 11:57 PM
Is it possible to implement secure boot without using trust zone for stm32u585.
without trust zone i want to use Boot lock, OTP, secure address like features.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-25 5:18 AM
Hi,
Yes, it is possible to implement secure boot without using TrustZone for STM32U585. The STM32U585 microcontroller supports a range of security features including Boot lock, OTP, and secure address space which can be used to implement secure boot.
The STM32Cube MCU Package provides a Secure Boot and Secure Firmware Update solution for STM32 microcontrollers. This solution is based on the open-source TF-M reference implementation.
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-29 4:05 AM - edited ‎2023-08-29 7:02 AM
Thanks for Response.
I would like to know can we port the SBSFU along with Secure Engine (STM32CubeExpansion_SBSFU_V2.6.2) of STM32H7 series to STM32U5?
The idea is to have a common bootloader for STM32U5 and STM32H7 based on SBSFU package provided for STM32H7(STM32CubeExpansion_SBSFU_V2.6.2) & trying to avoid using TF-M based package, since STM32H7 doesn't support TF-M