2017-05-11 3:58 AM
Hi,
i designed a flight controller board based on STM32F303. i have a weird problem where each time i assembled a complete board, initially there will be no problem and PC will be able to detect and connect with the board via USB VCP. but after a while, the board will be disconnected and USB VCP com port is not detected.
i have to resolder usb pins (PA11 pin32 & PA12 pin33) or reflow the whole board, test it again, no problem but after awhile USB VCP is missing again. if i repeat the whole reflow & retest eventually the USB VCP missing problem goes away.the board is a two layer PCB with HASL lead surface finish. did i get a faulty STM32F303 batch or should i have used immersion gold surface finish for better solder connection?
Please help me with this weird problem, thank you.#stm32 #usb #stm32f3 #vcpSolved! Go to Solution.
2017-05-29 9:07 AM
Hi,
i've found the problem. The USB data+ connection was pulled high to 5V with 1K5 resistor which is supposed to be pulled high to 3V3.
so i changed the resistor with 2K2.Thank you.
2017-05-13 1:03 PM
Hi guys,
Please help, thank you
2017-05-15 8:01 PM
Hi guys,
any advice please? i would very much appreciate it.
Thank you.
2017-05-29 9:07 AM
Hi,
i've found the problem. The USB data+ connection was pulled high to 5V with 1K5 resistor which is supposed to be pulled high to 3V3.
so i changed the resistor with 2K2.Thank you.
2020-10-06 10:31 AM
I'm also looking for the same device to record my game of Golf ball in the ground. Where can I get that?