Info USB CDC Device Descriptor
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-10-06 7:24 AM
Posted on October 06, 2015 at 16:24
Hi, I'm using STM32f407 for a USB project. I use CDC class for implementing USB device on my OLIMEX EVAL board.
This is my Device Descriptor:__ALIGN_BEGIN uint8_t USBD_DeviceDesc[USB_LEN_DEV_DESC] __ALIGN_END = {
0x12, /* bLength = 18 campi del Device Descriptor*/ USB_DESC_TYPE_DEVICE, /* bDescriptorType = 1*/0x00
, 0x02, /* bcdUSB = 2.00 */ 0x02, /* bDeviceClass: CDC */ 0x00, /* bDeviceSubClass */ 0x00, /* bDeviceProtocol */ USB_MAX_EP0_SIZE, /* bMaxPacketSize0 = 64 */ LOBYTE(USBD_VID), /* idVendor low byte = 0x83; essendo VID = 0x0483 (STMicroelectronics) */ HIBYTE(USBD_VID), /* idVendor high byte = 0x400 */ LOBYTE(USBD_PID), /* idProduct low byte */ HIBYTE(USBD_PID), /* idProduct high byte */0x00
, 0x02, /* bcdDevice = rel. 2.00 */ USBD_IDX_MFC_STR, /* Index of manufacturer string = 1 */ USBD_IDX_PRODUCT_STR, /* Index of product string = 2*/ USBD_IDX_SERIAL_STR, /* Index of serial number string = 3*/ USBD_MAX_NUM_CONFIGURATION /* bNumConfigurations = 1 */ }; /* USB_DeviceDescriptor */ My questions are: 1 - Text in red,which
parameters are?
2 - The position of the parameters are important? 3 - Why idVendor and idProductare
divided into low and high byte?
They must not
be passed
full
?
thank you all! #dev #stm32 #usb #cdc #desc
Labels:
- Labels:
-
USB
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-10-13 6:59 AM
Posted on October 13, 2015 at 15:59
Hi ragazzi.valerio,
The definition of parameters in the USB device descriptor is based on the definition in thehttp://sdphca.ucsd.edu/Lab_Equip_Manuals/usb_20.pdf
.Fields as bcdUSB, idvendor, idProduct and bcdDevice are of size 2. So they require 2 parameters in the array.The position of these parameters follow the previous spec as well (see Table 9-8).-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.