cancel
Showing results for 
Search instead for 
Did you mean: 

I'm trying to update the code on a STM32F407 MCU using OTA and the update is sent through MQTT. The issue is that it takes a long time to update, I was wondering if there was a way to decrease the time. Also, if it's better to use MQTT or something else.

JDhil.1
Associate
 
1 REPLY 1
Ozone
Lead III

Not much usable information.

The time is lost somewhere in the sequence chain of block reception, validity check, Flash programming, and response.

Check first where most time is spent.