cancel
Showing results for 
Search instead for 
Did you mean: 

How to sync usb device MSC with host

Jason927
Associate III

I'm already achieved a USBX-MSC class, and also a FileX in MCU local.

I know that using two file systems at the same time is not recommended, but still have some questions.

 

1. I implement the ux_deveice_msc.c as followed. Use PC-Windows to create a file such as my_test.txt to U-DISK, successfully and the local FileX will see the new file immediately.

UINT USBD_STORAGE_Read(VOID *storage_instance, ULONG lun, UCHAR *data_pointer,
                       ULONG number_blocks, ULONG lba, ULONG *media_status)
{
  UINT status = UX_SUCCESS;

  /* USER CODE BEGIN USBD_STORAGE_Read */
    UINT fxStatus = FX_SUCCESS;
    while (number_blocks--) {
        fxStatus = fx_media_read(sdioDisk, lba, data_pointer);
        if (fxStatus != FX_SUCCESS) {
            status = UX_ERROR;
            break;
        }
        data_pointer += sdioDisk->fx_media_bytes_per_sector;
        lba++;
    }
  /* USER CODE END USBD_STORAGE_Read */

  return status;
}

UINT USBD_STORAGE_Write(VOID *storage_instance, ULONG lun, UCHAR *data_pointer,
                        ULONG number_blocks, ULONG lba, ULONG *media_status)
{
  UINT status = UX_SUCCESS;

  /* USER CODE BEGIN USBD_STORAGE_Write */
    UINT fxStatus = FX_SUCCESS;
    while (number_blocks--) {
        fxStatus = fx_media_write(sdioDisk, lba, data_pointer);
        if (fxStatus != FX_SUCCESS && lba != 0) {
            status = UX_ERROR;
            break;
        }
        data_pointer += sdioDisk->fx_media_bytes_per_sector;
        lba++;
    }
  /* USER CODE END USBD_STORAGE_Write */

  return status;
}

UINT USBD_STORAGE_Flush(VOID *storage_instance, ULONG lun, ULONG number_blocks,
                        ULONG lba, ULONG *media_status)
{
  UINT status = UX_SUCCESS;

  /* USER CODE BEGIN USBD_STORAGE_Flush */
    if (fx_media_cache_invalidate(sdioDisk) != FX_SUCCESS || fx_media_flush(sdioDisk) != FX_SUCCESS) {
        status = UX_ERROR;
    }
  /* USER CODE END USBD_STORAGE_Flush */

  return status;
}

 

2. When I use local FileX to create a new file, and call function fx_media_flush, the Host PC-Windows can't see th new file until the usb reconnect. Seem windows explorer cache not fresh.

3. Based on point 2, I want to implement function USBD_STORAGE_Status, when some changes happend in local, return a UX_ERROR and media_status with Sense Key = UNIT ATTENTION (0x06), ASC/ASCQ = NOT READY TO READY CHANGE, MEDIA MAY HAVE CHANGED (0x28, 0x00). The purpose is let host reread the U-DISK's FAT32 table.

 

UINT USBD_STORAGE_Status(VOID *storage_instance, ULONG lun, ULONG media_id,
                         ULONG *media_status)
{
  UINT status = UX_SUCCESS;

  /* USER CODE BEGIN USBD_STORAGE_Status */
  UX_PARAMETER_NOT_USED(storage_instance);
  UX_PARAMETER_NOT_USED(lun);
  UX_PARAMETER_NOT_USED(media_id);
  UX_PARAMETER_NOT_USED(media_status);
  /* USER CODE END USBD_STORAGE_Status */

  return status;
}



I want to know if this method is feasible? THANK YOU!

 

1 REPLY 1
FBL
ST Employee

Hi @Jason927 

To better understand your setup, could you provide your full firmware setup to reproduce the issue?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL