Skip to main content
JinSQ
Visitor II
January 26, 2022
Question

How to operate a SD card with two partition using FILEX?

  • January 26, 2022
  • 0 replies
  • 721 views

I modified my project from filex demo in package STM32H7 AZURE, when i insert a SD card which has only one partiton, filex can read/write files on SD card. Then i format the SD card and create two partition, now filex cannot mount SD card. the error code is FX_MEDIA_INVALID. (The files system is FAT32)

------------------------------------------------------------

update: Formatting with exFAT can resvolue mount issue.Now I can mount SD card and read first partition, but accessing to second partiton is still pluzzed me.

This topic has been closed for replies.