2022-05-05 12:34 PM
i've alread tried these tutorial but doesnt work(https://controllerstech.com/stm32-usb-host-hid/).
the board schematic for stm32f407vet6 - https://stm32-base.org/assets/pdf/boards/original-schematic-STM32F407VET6-STM32_F4VE_V2.0.pdf
and some infos - https://stm32-base.org/boards/STM32F407VET6-STM32-F4VE-V2.0.html
2022-05-05 1:04 PM
"Doesnt work" is not very informative. Does anything work at all?
Can you pass enumeration of the mouse (read descriptors) ? Can you get raw report data from the mouse?
2022-05-05 1:42 PM
yes, anything works. i connect the mouse via usb port or via mcu pins and nothing respond (the led is always off). in these code i use a callback function for every data (x,y) and will be displayed in PC via uart.
i use the A725 sensor.
2022-05-05 2:19 PM
The LED always off can mean that the device does not receive power from the USB host.
Have you tried to connect a simple mouse instead of the sensor?
2022-05-06 5:17 AM
Yes, i'm using a gamer mouse for my project that have the A725 sensor. but i already tried a simple mouse, and have the same result. i think its the module that i have. i will try using only D- and D+ and not the Vbuss.