2019-07-01 9:49 AM
After I've loaded the BL then the FW i encountered the below scenarios:
1-Full chip erased 0xFF in the whole flash.
2-Garbage value in bank of FW.
3-BL code exist but FW code is erased.
I wounder why that happened?
some times making repeated power on/off several times makes the program starts on boot loader.from reading the flash the other bank is erased,I wonder why?
-In general may you refer me to application note or any document which illustrate the causes of flash corruption?
Thanks in advance.