2021-11-24 3:34 AM
2021-11-24 10:55 PM
@JAgni.1 Check the USB Port Pins are same and Clock Settings . In schematics check the MIC (Analog or Digital). If you have same target board working fine, Check once more .
If target board share the error then the it could be the cable or debugging connection issue
2021-11-25 4:22 AM
@Snara.2 Thank you for your quick reply. I have checked USB Port pins and clock settings. That error message is gone now, there was issue with USB cable. But still STM32F446RE not getting detected as USB Mic. I am using only mic node of X-CUBE package. I have ported Application/User files to my own project keeping Board support package,drivers as it is(hardware). Do I need to do any setting for USB enumeration? I have been stuck at this point for many days. I appreciate your help.
2021-12-06 4:19 AM
Hello,
I have resolved that USB enumeration issue. But using X-CUBE-USB-AUDIO package, I am not able to record any voice. Is there any utility that needs to be use to make this package work properly? Please help me. Thank you in advance.