Hello, I am using two USBs (one FS and one HS) as HID hosts. Both USBs work and read data from keyboard correctly but only when using 1 keyboard. When using two keyboards at the same time, many multiple presses are registered. Any idea why?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-06-30 5:11 AM
To clarify:
- MCU: STM32F205
- Code: HAL generated by Cube
- Multiple presses registered by function: USBH_HID_EventCallback
- 2x USB (FS,HS). both HID. both HOST
Problem:
- Many multiple presses registered when two keyboards are connected at the same time (happens for both of them) - not desired
- When any keyboard connected alone to one of USBs 1 press is only registered once - desired behaviour
Thanks for any ideas and help!
- Labels:
-
STM32F2 Series
-
USB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-06-30 5:41 AM
> Any idea why?
> Code: HAL generated by Cube
The keyboard driver is probably buggy and does not have properly instantiated multiple sets of state variables.
I am not going to dig deep here as I'm not interested in Cube, just casually met this once and my impressions are described in https://community.st.com/s/question/0D50X00009XkZ4KSAV/usb-host (can't give direct link to post courtesy of the crap salesforce ST insists on using instead of proper forum software; you have to click through "More" at the bottom as the thread is longer than 10 posts and my post is at the "3rd page").
JW