2025-09-09 11:45 AM - edited 2025-09-09 11:47 AM
I have an SPI slave running on STM32L4 in DMA mode. Here is the basic structure (simplified for this posting):
#define NSS (HAL_GPIO_ReadPin( SPI3_NSS_GPIO_Port, SPI3_NSS_Pin ))
#define BUFFERSIZE 32
uint8_t SpiTxBuffer[BUFFERSIZE], SpiRxBuffer[BUFFERSIZE];
typedef enum
{
Idle,
Wait,
Abort,
Done
} State_t;
State_t State = Idle;
int main(void)
{
/*
Usual MX boilerplate here.
*/
while(1)
{
switch (State)
{
case Idle:
if(!NSS)
{
if( HAL_SPI_TransmitReceive_DMA( &hspi, SpiTxBuffer, SpiRxBuffer,
BUFFERSIZE ) != HAL_OK )
{
Error_Handler();
}
State = Wait;
}
break;
case Wait:
if(NSS)
{
if( HAL_SPI_Abort_IT(&hspi) == HAL_OK)
{
State = Abort;
}
else
{
Error_Handler();
}
}
break;
case Abort:
break;
case Done:
DoSomethingWithTheData();
State = Idle;
}
DoSomethingElse(); /*Do some task while waiting for SPI to arrive*/
}
}
void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi)
{
State = Done;
}
void HAL_SPI_AbortCpltCallback(SPI_HandleTypeDef *hspi)
{
State = Done;
}In this circumstance, if the host (master) sends fewer bytes than expected and deactivates NSS, I detect this and abort the SPI exchange. However, the AbortCallback never gets called as evidenced by the fact that State never gets set to DONE.
Any ideas?
Edit: Fixed a typo
Solved! Go to Solution.
2025-09-11 2:01 PM
If I ignore the return value of HAL_SPI_Abort(), the subsequent HAL_SPI_TransmitReceive_DMA does not return HAL_OK so something strange is indeed going on.
I don't understand why the FIFO level bits are not going to zero. Shouldn't just 4 reads of the DR be enough to totally clear the FIFO? Just a comment; I'm still digging.
2025-09-11 2:24 PM
Once I get more info about the FIFO, not clearing, I'll open a new topic. The original question has been answered to my satisfaction.