2021-08-20 10:11 AM
Hello,
If I am using an external interrupt on a GPIO pin HAL_Delay() in my program's main() does not work.
while (1)
{
serprintf("Before HAL Delay");
HAL_Delay(500);
serprintf("After HAL Delay");
}"After HAL Delay" never happens. I've read a few threads that indicate that you should not use HAL_Delay() in the interrupt function, which is fine. I am not doing that.
If I disable the interrupt, the main loop works as expected.
2021-08-20 10:42 AM
>>If I disable the interrupt, the main loop works as expected.
Suggests that the EXTI IRQ handler doesn't satisfactorily clear the interrupting state, and it continuously re-enters.
Or something else going on in your unspecified STM32 system more generally.
2021-08-20 10:47 AM
void EXTI4_IRQHandler(void)
{
/* USER CODE BEGIN EXTI4_IRQn 0 */
VL53L3CX_SimpleRanging_Int();
/* USER CODE END EXTI4_IRQn 0 */
HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_4);
/* USER CODE BEGIN EXTI4_IRQn 1 */
/* USER CODE END EXTI4_IRQn 1 */
}Should I be doing more than the this? This function is generated code from CubeMX.
2021-08-20 1:04 PM
It's all very superficial.
Perhaps have a count so you can see how often it passes. If it enters several hundred thousand times a second then nothing else will likely run.
The tail-chaining methods will basically block execution of foreground code. You basically get an "interrupt storm", and saturate the processor.
You should check the reporting in the NVIC/EXTI to ensure nothing is pending as you leave.
2021-08-20 1:07 PM
Good point. Sorry, I should have indicated the interrupt is driven by a piece of hardware of 30Hz. So it's not very fast.
The last statement you made was interesting "You should check the reporting in the NVIC/EXTI to ensure nothing is pending as you leave."
I would like to learn how to do this either way.