cancel
Showing results for 
Search instead for 
Did you mean: 

Getting started FFT STM32?

Endika Caño de Miguel
Associate II
Posted on March 12, 2018 at 12:18

Hello everyone:

I have to make the FFT on my STM32L4 32KC board and I don�t know where to start. 

Sound is coming from the outside and I have to make the FFT.

Any tips would help a lot.

I�ve looking on the net for help, but everything was a little to messy for me. 

I�m pretty new to micro-controlers, so there are many things that I ignore unfortunately.

Thanks in advance for your time and help.

#stm32 #fft #l4 #cmsis #dsp
This discussion is locked. Please start a new topic to ask your question.
15 REPLIES 15
Posted on June 25, 2018 at 17:49

Did you look at the links provided by

st.mcu

‌ ?

Did you see

https://community.st.com/0D70X000006SwKPSA0

?

Why would an FFT on an STM32F4 differ from an FFT on any other Cortex-M4?

Have you looked at the standard CMSIS stuff?

CMSIS Intro:

https://www.keil.com/pack/doc/CMSIS/General/html/index.html

https://www.keil.com/pack/doc/CMSIS/DSP/html/index.html

https://www.keil.com/pack/doc/CMSIS/DSP/html/arm_fft_bin_example_f32_8c-example.html

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Posted on June 25, 2018 at 18:11

evading wrote:

FFT single point calculation

What do you mean by 'single point'?

Surely, a single point is just an impulse - so the FFT is known?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Posted on June 26, 2018 at 07:24

What do you mean by 'single point'?

Perhaps he is meaning something like the Goertzel algorithm, to calculate individual terms (spectral 'points') ?

There is no specific example for that in ARM's DSP-Lib, but surely elsewhere on the web.

And as said, these algorithms are hardware-independant.

Amel NASRI
ST Employee
Posted on June 26, 2018 at 11:52

Hi,

I recommend you to have a look to the tutorial

https://community.st.com/0D50X00009bMMAwSAO

created by

Majerle.Tilen

‌.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on June 27, 2018 at 16:11

Hi,

I want just to customize the arm_cfft_f32 to get some specific elements 

of the the complex data buffer and calculate its FFT value.

arm_cfft_f32 ( const arm_cfft_instance_f32 * S,

float32_t * p1,

uint8_t ifftFlag,

uint8_t bitReverseFlag

)

Otherwise, any sinus generated data buffer can be used for testing ? at least to be sure of the FFT results ?

Thanks.

Posted on June 28, 2018 at 08:21

I never hacked the arm_cfft functions, but surely you can adapt it to drop the calculations you don't need.

I used to calculate all frequencies, to evaluate one (or more) spectral components in relation to the others.

...any sinus generated data buffer can be used for testing ? at least to be sure of the FFT results ?

Yes. This is recommended.

The ARM example comes with a reference input signal, however not a 'sinus' wave shaped.