cancel
Showing results for 
Search instead for 
Did you mean: 

FreeRTOS ulTotalRunTime should be defined as volatile

Mohammad A
Senior

After failing to view run time results of tasks in FreeRTOS, found this blog from Atollic which describes ulTutoralRunTime in tasks.c has to be defined as volatile otherwise it won't be updated whenever optimization is above -O0 .

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Piranha
Chief II

Above -O0 many debugging related things break apart...

From gcc documents:

Optimize debugging experience. -Og should be the optimization level of choice for the standard edit-compile-debug cycle, offering a reasonable level of optimization while maintaining fast compilation and a good debugging experience. It is a better choice than -O0 for producing debuggable code because some compiler passes that collect debug information are disabled at -O0.

Like -O0, -Og completely disables a number of optimization passes so that individual options controlling them have no effect. Otherwise -Og enables all -O1 optimization flags except for those that may interfere with debugging

KnarfB
Super User

> ulTutoralRunTime in tasks.c has to be defined as volatile

This may be a Atollic TrueStudio specific requirement for updating their GUI FreeRTOS Task List view.

In general, no changes are required and the code works out-of-the-box when using the FreeRTOS supplied vTaskGetRunTimeStats function.

Set up an up-counting timer running at a frequency considerably higher than the FreeRTOS tick, say TIM2 at 1 MHz.

Activate in FreeRTOSConfig.h:

#define configGENERATE_RUN_TIME_STATS            1
#define configUSE_TRACE_FACILITY                 1
#define configUSE_STATS_FORMATTING_FUNCTIONS     1

Override the _weak defaults by implementing:

void configureTimerForRunTimeStats(void)
{
	HAL_TIM_Base_Start(&htim2);
}
 
unsigned long getRunTimeCounterValue(void)
{
	return __HAL_TIM_GET_COUNTER(&htim2);
}

And now you can periodically read-out the statistics in a tasks by:

char pcWriteBuffer[256];
vTaskGetRunTimeStats(pcWriteBuffer);

and send the results to an UART or other interface. You get output like

...
defaultTask     24120810                8%
IDLE            270603162               91%
Tmr Svc         58              <1%

Btw: There is no need to setup an additional timer interrupt as suggested in that tutorial. That creates only overhead...

Even -Og optimizes out variables and does a few things, which can make debugging cumbersome. Anyway it's not what your original topic is about. The FreeRTOS doesn't need that variable to be volatile, it's only that viewing tool under specific optimization levels, that needs it.