Skip to main content
SYako
Associate III
April 15, 2021
Solved

FreeRTOS + UART + DMA stops working on second debug session

  • April 15, 2021
  • 2 replies
  • 1112 views

On first debug session everything works fine. However on second and beyond session dma stop working.

Hardware: custom stm32l4p5cet based board, original ft232 uart bridge, stlink v2.

CubeMX settings: UART with DMA on RX and TX (RX in circular mode), Global interrupt enabled with priority 5.

Code:

Start DMA returning HAL_OK:

HAL_UART_Receive_DMA(&huart2, serial_data, 128);

Task to put data from uart in to message queue:

static uint16_t tail;
 
void serial_input_task(void *arg)
{
	for (;;) {
		uint16_t len = 128 - huart2.hdmarx->Instance->CNDTR;
		while (len - tail) {
			uint8_t tmp = serial_data[tail];
			osMessageQueuePut(at_input_queue, (const void*) &tmp, 0, 0);
			tail++;
			if (tail >= 128)
				tail = 0;
		}
		osDelay(1);
	}
}

task to read message queue and process data:

static uint8_t at_serial_input[128];
 
void input_task(void *arg)
{
	uint32_t count;
	while (1) {
		count = osMessageQueueGetCount(input_queue);
		for (uint32_t i = 0; i < count; i++)
			osMessageQueueGet(input_queue,(void*) &serial_input[i], 0, 0);
		if (count)
			input(serial_input, count); //handle raw data from uart
	}
}

function input never get called, for testing purposes I added RxCpltCallback to light up led. Never get called or light up, even in first debug session.

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
	HAL_GPIO_WritePin(LED2_GPIO_Port, LED2_Pin, GPIO_PIN_SET);
}

This topic has been closed for replies.
Best answer by SYako

Hi, after deep analysis, error was caused by external device that was connected to uart, and generated errors on RX line.

2 replies

Walid ZRELLI
Visitor II
April 26, 2021

Hello @SYako​,

Could you please share you project for further check ?

Thanks in advance.

Walid.

SYako
SYakoAuthorBest answer
Associate III
April 29, 2021

Hi, after deep analysis, error was caused by external device that was connected to uart, and generated errors on RX line.