Executing HAL_I2C_Master_Transmit_IT function holds SCL low.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-01 7:41 AM
Hi,
I found in my search there is a similar question that went unanswered. This may be a newb question, but I'm stuck on it.
What I have found is that when executing HAL_I2C_Master_Transmit(), the data transfer happens as expected. (I happen to have green LEDs hanging on GPIO). When I execute HAL_I2C_Master_Transmit_IT(), only the 7-bit address is sent, and the Master (this program) continues to hold the SCL line low.
If someone could explain what I am doing wrong with the HAL_I2C_Master_Transmit_IT() program, that would be much appreciated!
//Turn on the two green LEDs on the LTC4306's GPIO
data[0] = 0x01;
data[1] = 0b00001111;
status = HAL_I2C_Master_Transmit(&hi2c1, ltc4306_Address, data, 2, 1 );
//Turn off the two green LEDs on the LTC4306's GPIO
data[0] = 0x01;
data[1] = 0b00111111;
status = HAL_I2C_Master_Transmit(&hi2c1, ltc4306_Address, data, 2, 1 );
//Turn on the two green LEDs on the LTC4306's GPIO
data[0] = 0x01;
data[1] = 0b00001111;
status = HAL_I2C_Master_Transmit_IT(&hi2c1, ltc4306_Address, data, 2 ); //This returns HAL_OK... but the master (this program) is holding SCL low after having transmitted the 7-bit address.
HAL_I2C_MasterTxCpltCallback(&hi2c1); // SCL still being held low after execution of this line. Doesn't seem to help.
- Labels:
-
I2C
-
STM32Cube MCU Packages
-
STM32G0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-18 2:04 AM
I had similar problem. If you had something like that:
uint8_t fn{
uint8_t data[2];
data[0] = 0x01;
data[1] = 0b00001111;
status = HAL_I2C_Master_Transmit(&hi2c1, ltc4306_Address, data, 2, 1 );
data[0] = 0x01;
data[1] = 0b00111111;
status = HAL_I2C_Master_Transmit(&hi2c1, ltc4306_Address, data, 2, 1 );
data[0] = 0x01;
data[1] = 0b00001111;
status = HAL_I2C_Master_Transmit_IT(&hi2c1, ltc4306_Address, data, 2 );
return 0;
}
In the moment, when you execute return line, you pop fn function pointer from stack. i2c takes data from different place in memory and NACK on SDA occurs -> transmitting is stopped.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-04-07 10:20 PM
You probably missed the I2C1 interrupt handler function. I had a similar problem when executing this function HAL_I2C_Master_Transmit_IT(). After I added the interrupt handler function, the problem was fixed.
I added I2C1 interrupt handler in to the "stm32fxxx_it.c" file as below:
/* External variables --------------------------------------------------------*/
extern I2C_HandleTypeDef hi2c1;
void I2C1_IRQHandler(void)
{
if (hi2c1.Instance->ISR & (I2C_FLAG_BERR | I2C_FLAG_ARLO | I2C_FLAG_OVR)) {
HAL_I2C_ER_IRQHandler(&hi2c1);
} else {
HAL_I2C_EV_IRQHandler(&hi2c1);
}
}
And don't forget to add I2C1 interrupt enable to this function HAL_I2C_MspInit(I2C_HandleTypeDef* hi2c)
HAL_NVIC_SetPriority(I2C1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(I2C1_IRQn);
Hope it helps.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-04-07 10:35 PM
You probably missed the I2C1 interrupt handler function. I had a similar problem. After I added the interrupt handler function, the problem is fixed.
I added the interrupt handler to "stm32f0xx_it.c" file as below. (I use STM32F072RBT6 chip)
void I2C1_IRQHandler(void)
{
if (hi2c1.Instance->ISR & (I2C_FLAG_BERR | I2C_FLAG_ARLO | I2C_FLAG_OVR)) {
HAL_I2C_ER_IRQHandler(&hi2c1);
} else {
HAL_I2C_EV_IRQHandler(&hi2c1);
}
}
And also added I2C1 interrupt initialization to HAL_I2C_MspInit() function as below
void HAL_I2C_MspInit(I2C_HandleTypeDef* hi2c)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(hi2c->Instance==I2C1)
{
__HAL_RCC_GPIOB_CLK_ENABLE();
/**I2C1 GPIO Configuration
PB8 ------> I2C1_SCL
PB9 ------> I2C1_SDA
*/
GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF1_I2C1;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* Peripheral clock enable */
__HAL_RCC_I2C1_CLK_ENABLE();
/* I2C1 interrupt Init */
HAL_NVIC_SetPriority(I2C1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(I2C1_IRQn);
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-05-04 3:49 PM
I am using STM32H745I-DISCO board. STM32CubeMX v6.5.0. generates interrupt handlers:
void I2Cx_EV_IRQHandler(void)
void I2Cx_ER_IRQHandler(void)
and MspInit function:
void HAL_I2C_MspInit(I2C_HandleTypeDef* hi2c)

- « Previous
-
- 1
- 2
- Next »