Error when runing USB_OTG_FS with RTOS for pendrive application.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-12 1:47 AM
Hello Everyone,
First of all I have run the project with STM32H745I + USB_OTG_FS + FATFS + MSHC for the pendrive application and it runs without any error, I am able to create a file, directrory & write into the file.
But when I add FreeRTOS in the same combination of existing project I can only mount the USB after that I stuck in HardFault handler. I don't know what the exact setting I have to do with FreeRTOS.
If anyone have idea please help me out.
Thanks!
Solved! Go to Solution.
- Labels:
-
FatFS
-
STM32H7 series
-
USB
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-19 10:07 PM
Hello Everyone,
I have solved this problem, There were some settings to be done with FreeRTOS feature.
Missing settings were:
In USB_HOST_M7 Mode USBH_PROCESS_STACK_SIZE value should be 8*128 words with no check. USBH_PROCESS_PRIO value can be normal(default) or below normal. Another setting will be default.
In FATFAS_M7 setting set USE_LFN to Enable LFN with dynamic working buffer on the HEAP. USE_STRFUNC will be disabled.
For clock setting you can use the below parameters:
/* PLL3 for USB Clock */
PeriphClkInitStruct.PLL3.PLL3M = 25;
PeriphClkInitStruct.PLL3.PLL3N = 336;
PeriphClkInitStruct.PLL3.PLL3FRACN = 0;
PeriphClkInitStruct.PLL3.PLL3P = 2;
PeriphClkInitStruct.PLL3.PLL3R = 2;
PeriphClkInitStruct.PLL3.PLL3Q = 7; /* 336/7 =48Mhz*/
The timer on which FreeRTOS works Keep their priority at 4 and the priority of USB global interrupt is lower than 4 or can keep 15.
Thanks!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-19 10:07 PM
Hello Everyone,
I have solved this problem, There were some settings to be done with FreeRTOS feature.
Missing settings were:
In USB_HOST_M7 Mode USBH_PROCESS_STACK_SIZE value should be 8*128 words with no check. USBH_PROCESS_PRIO value can be normal(default) or below normal. Another setting will be default.
In FATFAS_M7 setting set USE_LFN to Enable LFN with dynamic working buffer on the HEAP. USE_STRFUNC will be disabled.
For clock setting you can use the below parameters:
/* PLL3 for USB Clock */
PeriphClkInitStruct.PLL3.PLL3M = 25;
PeriphClkInitStruct.PLL3.PLL3N = 336;
PeriphClkInitStruct.PLL3.PLL3FRACN = 0;
PeriphClkInitStruct.PLL3.PLL3P = 2;
PeriphClkInitStruct.PLL3.PLL3R = 2;
PeriphClkInitStruct.PLL3.PLL3Q = 7; /* 336/7 =48Mhz*/
The timer on which FreeRTOS works Keep their priority at 4 and the priority of USB global interrupt is lower than 4 or can keep 15.
Thanks!