2023-01-22 9:52 AM
I am attempting to use TraceX in my NetXDuo application. But when I enable TraceX in the Software Packs of CubeIDE (TX_ENABLE_EVENT_TRACE) I get compiler errors in all of the calls to save a tracex event. The macros that defines the calls to tracex services appear in nx_api.h, but are not defined, and hence the _nx_trace_event_ service is never defined.
I saw a discussion of this same issue over in the Renesis community where a workaound fixed the compiler issue.
But t his workaround did not fix the STM code.
Can anyone suggest something that may help?
Thanks,
MikeH
Solved! Go to Solution.
2023-03-07 5:16 AM
It appears that the example code that I had used as the basis of this application was faulty. (It was apparently from an early CubeIDE example). I completely rebuilt the application using the Nucleo-H723 Nx_TCP_Echo_Server application from the Git download.
https://github.com/STMicroelectronics/x-cube-azrtos-h7
After help from Zuhair, and a LOT of watching the Workshops...
https://www.youtube.com/playlist?list=PLnMKNibPkDnGxMITHhhRqbT0-2egHq0D0
...I was able to configure the example to work properly and to generate TraceX functionality!
This is a very lengthy process due to the MANY modifications that must be made to the examples provided by ST. I highly recommend that ST provide a "ready-to-run" version of these examples so that you don't loose developers who don't have the time or patience to spend plugging through the (partial) details provided by the (very well done) workshops.
In summary, I now have TraceX working on a TCP Server application on a Nucleo H723 board. I find TraceX to be marginally helpful due to its clunky GUI and somewhat limited functionality. Hopefully it will help me debug the issues that I now have with network reliability and stability.
Thanks again Zuhair for your guidance!
MikeH
2023-02-14 2:27 AM
Hi MikeH,
I haven't reproduced your issue can you please provide more details on:
By the way can you check that the NetXDuo trace files (nx_trace_*) are added to your project when enabling TraceX support
Regards
2023-02-14 10:11 AM
ZA,
Device STM32F723ZGTx
Board: NUCLEO-H723ZG
X-CUBE-AZRTOS Versions
My program is based off of the Nx_TCP_Echo_Server example. I have added additional user code which forwards commands received from a TCP client to USART2. The response received from the USART is then forwarded back to the client. This all works as expected, except that occasionally the network connection is dropped. I need to use TraceX to debug this issue.
By the way can you check that the NetXDuo trace files (nx_trace_*) are added to your project when enabling TraceX support
I don't see any nx_trace_ code inserted into main.c, app_nextduo.c, or app_azure_rtos.c. I manually inserted the following into app_threadx.c per the training video.
TX_THREAD thread_ptr;
#define TRACEX_BUFFER_SIZE 64000
uint8_t tracex_buffer[64000] __attribute__ ((section (".trace")));
/* USER CODE END PV */
...and
tx_trace_enable(&tracex_buffer,TRACEX_BUFFER_SIZE,30);
/* USER CODE END App_ThreadX_Init */
Thanks for the help.
MikeH
2023-02-15 3:24 AM
2023-02-15 7:53 AM
Thanks Zouhair. I'll give this a try over the next few days and report back.
I did install V3.0 X-CUBE-AZRTOS-H7 and now see the TraceX support files as shown in your screenshot.
Thanks,
MikeH
2023-02-19 9:11 AM
Zouhair,
I was able to get your sample code working and was able to capture TraceX data and view it in the TraceX app. Thanks for that.
However, I did run into several issue when trying to incorporate TraceX into my application (based on the NX_TCP_Echo_Server example code).
#define NX_APP_MEM_POOL_SIZE 0x8200
Thanks again for your help.
Mikeh
2023-02-20 6:33 AM
Please find below my comments/answers:
1-I ran out of byte_pool memory when allocating all of the services in my NetxDuo application.
As mentioned in readme file some changes are required when changing the NX_PACKET pool size or address. The NX_PACKET start address (0x24048000) used in this example allows only pool size < 32KB so you you need to set/update start address as follows:
.tcp_sec (NOLOAD) : {
. = ABSOLUTE(0x24030000);
*(.RxDecripSection)
. = ABSOLUTE(0x24030060);
*(.TxDecripSection)
} >RAM_D1 AT> FLASH
.nx_data 0x24030200 (NOLOAD):
{
*(.NetXPoolSection)
} >RAM_D1 AT >FLASH
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.BaseAddress = 0x24030000;
MPU_InitStruct.Size = MPU_REGION_SIZE_64KB;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
2.CubeIDE doesn't always save a manually change value for NetXDuo memory pool size when it is changed in the CubeIDE GUI , even after Code Generation
Do you have same behavior with STM32CubeMX 6.7.0 ?
3-Your sample project did not include any BSP support code
BSP support is not managed by X-CUBE-AZRTOS and BSP files should be added manually by user or using .extSettings file which allows to add paths and files to project:
[ProjectFiles]
HeaderPath=..\..\..\..\..\..\Drivers\BSP\STM32H7xx_Nucleo
[Others]
HALModule=
[Groups]
Drivers/BSP/STM32H7xx_Nucleo=../../../../../../Drivers/BSP/STM32H7xx_Nucleo/stm32h7xx_nucleo.c;
2023-02-20 8:42 AM
Zuhair,
Thanks so much for your continued assistance.
I made the memory allocation modifications that you recommended. But I still get a Hard Fault when the byte_pool allocation attempts to allocate greater that 32kbytes.
Here is what I modified.
/* Allocate the memory for TCP server thread */
if (tx_byte_allocate(byte_pool, (VOID **) &pointer,2 * DEFAULT_MEMORY_SIZE, TX_NO_WAIT) != TX_SUCCESS)
Could there be some other setting that limits the allocated memory to 32kbytes?
thx
MikeH
2023-02-20 9:00 AM
can you share your example if it's possible ?
2023-02-20 9:06 AM
Do you have an email address that I could send it to?