2019-11-24 6:43 AM
hi
i need help to have dual Micro SD in one Mass Storage Device in H743 for see two micro sd in pc from one usb
project use two sdio 1 & 2 , devise fs and mass storage
it work correct for every micro sd separately but not work together
in code last init micro sd work
this page source for one sd, mass storage that i use
https://microtechnics.ru/en/stm32-i-usb-mass-storage-sd-card/#comment-16577
2019-11-24 8:31 AM
Typically you'd have the MSC report multiple LUN, each would report unique INQUIRY and CAPACITY information, and the you'd have two unique SDMMC instances dispatched based on decoded LUN from the SCSI packets.
2019-11-24 8:40 AM
i am beginner in it can you Explain more
thanks
2019-12-11 1:11 AM
i change Lun and now i see 2 drive of Mass Storage but all drive present just one sd card
MX_GPIO_Init();
MX_SDMMC1_SD_Init();
MX_SDMMC2_SD_Init();
// MX_FATFS_Init();
if((FATFS_LinkDriver(&SD_Driver, RAMpath) == 0) && (FATFS_LinkDriver(&SD2_Driver, SDpath) == 0))
{
MX_USB_DEVICE_Init();//for sdio1
HAL_SD_Init(&hsd1);//for sdio1
//MX_USB2_DEVICE_Init();//for sdio2
HAL_SD_Init(&hsd2);// for sdio2
/* USER CODE BEGIN 2 */
2019-12-11 10:36 PM
in this code hsd1 (micro sd 1) appear in two drive if i change init hsd2 with hsd1, micro sd 2 appear in two drive
any one have idea ?!