Custom BootLoader jump to FreeRTOS application
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-19 1:23 AM
Hi all,
I've develop a specific bootloader which calling my application.My application is based on FreeRTOS.When the application starts after the jump, the firmware crashes in hardfault.It works fine when I don't use the FreeRTOS scheduler.I've tested my application (with FreeRTOS enabled) by loading it with the debugger and it works fine.FreeRTOS starts their tasks by calling SVC.Then, i've try also to replace the FreeRTOS scheduler starting by a simply __asm volatile (''svc 0'') and I reproduce the same issue.The application address is 0x0800C000.Like clive suggested, I have use a system call in my bootloader :void SVC_Handler(void){ pFunction Jump_To_Application; uint32_t JumpAddress; /* Jump to user application */ JumpAddress = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4); Jump_To_Application = (pFunction) JumpAddress; __disable_irq(); /* Initialize user application's Stack Pointer */ __set_MSP(*(__IO uint32_t*) APPLICATION_ADDRESS); Jump_To_Application();}I've checked the VECT_TAB_OFFSET in system_stm32f4xx.c to set it to 0xC000.Can anybody help me ?Thanks a lot,Pascal #stm32-freertos- Labels:
-
FreeRTOS
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-20 2:15 AM
''I simplify my application to not use FreeRTOS but simply call SVC at the beginning (__asm volatile(''svc 0'')).''
Why are you doing this? The 'SVC' is the ISR that handles context (task) switches in FreeRTOS. Without setting up tasks, there is not point calling the SVC ''SVCall - A supervisor call (SVC) is an exception that is triggered by the SVC instruction. In an OS environment, applications can use SVC instructions to access OS kernel functions and device drivers.'' ''The HardFault Handler is called immediatly.'' This is expected - unless the SVC ISR has been set correctly - it will cause a hardfault. ''It looks like that no handler will be load for treating SVC interrupt.'' That is correct in this circumstance. ''How can I verify that the vector table is loaded?'' Not sure why you are asking this. I think you do not understand what is happening. The Vector table should contain the 'default' ISR to call when there is an Interrupt. Some IRQs may be disabled (but still have a valid entry in the vector table). I do not understand what you are trying to do? Have you managed to start the application from the bootloader? Why are you changing the code in the application? ''I've disabled SysTick at starting in my application. Nothing change, I still have the same issue.'' So you are getting a HardFault when starting the application. Debug it.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-20 2:16 AM
Hi,
If I understand your code correctly, you are jumping from your bootloader to your application in context of SVC handler. vPortStartFirstTask function of Freertos calls SVC instruction, but you probably are doing it still inside the SVC handler which results in usage fault for which you probably don't have handler thus you end up in hard fault. check the xPSR's LSB bits upon jump to your application to see whether my hypothesis is right and if so, don't jump in SVC context.brkarel- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-20 2:33 AM
Sorry,
I see that I'm not so clear in my explanation and tests.I modify and simplify the starting of my application to see if SVCHandler will be call by launching the svc call.It's just a test. I will re-enable FreeRTOS after.And, it works fine when I load it and start it with the debugger.The SVCHandler is called by svc calling.As you say, I need to Initialize FreeRTOS tasks before the SVC called. I'm agree with you.The OS can't works with SVC call without initialize the tasks.But, by this test, I just want to know if the interrupts works fine after the jump.Normally, when the firmware makes a svc call the SVC Handler process it to extract parameters and switch context.But, in all cases the SVC Handler is called. I'm right ?Best regards,Pascal- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-20 2:42 AM
Hi Karel,
No, my BootLoader do not switch in SVC context (that's what I try at the beginning but avoid that now).Now, my BootLoader simply jump at application address after disable IRQ.Thanks for your help.Pascal- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-20 2:49 AM
Hi Karel,
The xPSR is set to 0 before jumping to application.Thanks,Pascal- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-20 7:55 AM
Hi all,
After some debugs I found the problem.In fact, the problem comes with the portDISABLE_INTERRUPTS macro of FreeRTOS.This macro calls the ulPortSetInterruptMask function : __asm volatile \ ( \ '' mrs r0, basepri \n'' \ '' mov r1, %0 \n'' \ '' msr basepri, r1 \n'' \ '' bx lr \n'' \ :: ''i'' ( configMAX_SYSCALL_INTERRUPT_PRIORITY ) : ''r0'', ''r1'' \ );FreeRTOS never call the portENABLE_INTERRUPTS to reset the BASEPRI before launch the SVC call???Have you an idea?Best regards,Pascal- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-20 8:19 AM
Some other related threads to connect some of the dots. The SVC example was a stab at having an RTOS with USER mode code get into SYSTEM mode for the transition.
https://community.st.com/0D50X00009XkbZhSAJ
https://community.st.com/0D50X00009Xkfb1SAB
https://community.st.com/0D50X00009Xka1fSAB
EDIT: Fixed links within forum after transition to Jive.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-22 1:14 AM
Thanks Clive for sharing these,
As I understand by reading your links, you suggest me to jump very early in the bootloader code after storing the address value to jump in RAM and Reset the processor?And then, the application will start very soon without any contaminated initialization.I think this will be a good idea.I will try this today.Best regards,Pascal- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-23 12:20 AM
I've implemented the modification with a MagicRAM and a systemReset.
It works well now !!!I want to thank you a lot Clive for your great support.Best regards,Pascal- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-16 5:50 AM
I'm facing the same problem on a custom board based on a STM32F767ZI microcontroller.
It seems like the links are dead, is there any other place where I can found a solution to the problem?
Thanks.