cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX FileX Maximum SRAM Disk Size

matt-crc
Senior III

Hello,

Why is there a limitation to the maximum Disk space in FileX?  256K is too small.  I would like to allocate 64Mbytes.

mattcrc_0-1740030478318.png

6 REPLIES 6
Saket_Om
ST Employee

Hello @matt-crc 

This is a hardware limitation. Please check the datasheet of your device. 

Saket_Om_0-1740049104126.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om
matt-crc
Senior III

Hi @Saket_Om 

I did and the memory is available.  I highlighted the available memory on the datasheet

mattcrc_0-1740053118943.png

 

Hello @matt-crc 

This is not an embedded SRAM. It concerns the FMC (Flexible external memory controller) peripheral which can control an external SRAM.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om
matt-crc
Senior III

hi @Saket_Om 

ok, but i find it very strange that FileX can be configured to use the FMC with the external Flash (Nor/Nand) without that limitation, but it can't use the very same FMC for a RAM disk... 

Yes, doesn't make sense to me either, should be able to use the SDRAM, and however large that is, less the offset into it.

Perhaps SRAM DISK is too specific, and there should be an SDRAM-DISK, or a more generalized RAM-DISK

@STTwo-32 please flag this for consideration/review for parts supporting external memory and/or SDRAM enabled, and an "Address" field in the user interface.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hello @Tesla DeLorean 

I reported your request internally. 

Internal ticket number: 203748 (This is an internal tracking number and is not accessible or usable by customers).

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om