2025-09-15 9:05 AM
I’m using an STM32 board to drive an SSD1322 128×64 OLED display with my own driver library. It used to work fine without issues. Without changing the code, the display suddenly became completely unresponsive.
- Power supply shows 0A current draw (normally it used to pull around ~0.3A).
- During debug, I noticed something strange: inside MX_GPIO_Init() the code enters, but it hangs at
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
and never progresses beyond that line.
I double-checked all hardware connections multiple times, nothing seems wrong.
When I swapped to another STM32 board of the same model, everything worked again without any changes.
This makes me suspect a hardware fault on the original board (possibly ESD damage).
My questions:
- What should I pay special attention to when debugging this kind of issue?
- How can I pinpoint the exact root cause (e.g., RAM/stack corruption, HardFault analysis, hardware measurements)?
- What’s the recommended way to solve this and prevent it in the future (ESD protection, design practices, etc.)?
2025-09-15 9:16 AM
> What should I pay special attention to when debugging this kind of issue?
You cannot "debug" a "dead" or "sick" cpu , to find out, why its "sick".
You only can prevent it, never let an ESD on a pin...
see, what our new friend telling:
2025-09-15 9:25 AM - edited 2025-09-15 9:27 AM
@durna wrote:it hangs at
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
Odd that it should hang there - that's just writing a constant value into a structure element.
Shouldn't have any hardware dependency at all.
But, if it has been hit by an ESD, then that does put it firmly into undefined behaviour territory ...
2025-09-15 10:25 AM
Hello @durna ,
@durna wrote:
- What’s the recommended way to solve this and prevent it in the future (ESD protection, design practices, etc.)?
Many parameters come into account for ESD protecting, design practices. I advise you to refer to ST's guidelines AN1709, AN5612) for detailed ESD design, routing tips and recommendations improving the ESD protection.