cancel
Showing results for 
Search instead for 
Did you mean: 

copy and run a bootloaderfunction to RAM memory

garzarolli
Associate II
Posted on March 11, 2010 at 16:55

copy and run a bootloaderfunction to RAM memory

#activation-internal-bootloader
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
damh
Associate II
Posted on May 17, 2011 at 13:43

I don't know the ride7 toolchain, but the simple internal bootloader can do that.

1) set BOOT0=VCC, BOOT1=GND

2) connect PA9==USART1_TX, PA10==USART1_RX

3) reset the stm32

4) send 0x7F from PC

5) receive ACK from BOOTLOADER

Rest can be read in AN2606.

Tomas DRESLER
Senior II
Posted on May 17, 2011 at 13:43

I guess you needed a little bit different answer:

create such C function in separate file and configure the linker to place the code content of this file into RAM (maybe in RIDE project explorer, maybe by hand-editing the linker file - I don't remember exactly now).

Other compilers use something like __ramfunc or #pragma((__section__ = ''.RAM'')) etc. Please look in the GCC documentation for placing code into RAM, it's there, but well hidden ;)