cancel
Showing results for 
Search instead for 
Did you mean: 

Clock source for OTG_HS and its USB_OTG_EMBEDDED_PHY

Emelm.1
Associate

Which clock is used for clocking the OTG_HS and its USB_OTG_EMBEDDED_PHY while in FS mode? Is it Fvco / PLLQ?

stm32f4

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User

It's not very clear from the RM, but most of the OTG modules runs probably out of the AHB clock, with only a synchronizer/interface portion running at the PHY clock, which comes, as you've said, from Q output of PLL (aka 48MHz clock).

Don't enable the ULPI clock in RCC. Note, that it's enabled by default in the LP version of enable registers.

JW

TDK
Super User

In external PHY mode, PLLQ isn't needed at all, so unlikely that the peripheral is using this clock.

If you feel a post has answered your question, please click "Accept as Solution".
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.