Circular buffers and Algobuilder
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-10-10 8:29 AM
new to algobuilder.
I want to have a float input circular buffer that then goes through an IIR filter. When I add both to algobuilder I can't seem to wire the circular buffer to the IIR filter block, presumably as the circular buffer output bus width is showing as a bus with the number of outputs as the number of elements in the circular buffer (qty 10) when the IIR is single float input.
How do I extract one float from the circular buffer at an index reference point using algobuilder?
Labels:
- Labels:
-
STM32CubeIDE
-
STM32CubeMX
0 REPLIES 0