Skip to main content
slime
Associate II
September 23, 2022
Question

Cannot switch between USB device and USB host mode on STM32H7A3-nucleo without cycling power

  • September 23, 2022
  • 1 reply
  • 1034 views

I am using a stm32h7a3-nucleo board to do proof of concept of this MCU supporting both USB Host as a MSD and USB Device as CDC. Using code from ST sample projects, it is setup to go to host mode if user button is held after a board reset. Both host and device modes work,

If device mode is selected after reset, then later the user resets the board, and tries to put it to host mode, the device does not properly init the USB drive connection. Since both modes start after a board reset, why do I need to pull power supply from the board to get USB host to work again? It does not matter if the USB drive is plugged in or not at the time of reset.

This topic has been closed for replies.

1 reply

ST Technical Moderator
September 26, 2022

Hello @slime​ ,

Do you have a pullup on the line? Use internal pull-ups on the ID pin, if there's no external one.

You need to stop ("xxxDeinit") the stack in one mode, and switch the mode. Then start the whole stack of the other mode, when the ID pin state changes.

If my answer satisfy your need, please select it as Best so that this thread will marked as solved.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks