cancel
Showing results for 
Search instead for 
Did you mean: 

Can USARTs with non default pins be used for accessing the bootloader

CR.11
Associate

The question at https://community.st.com/s/question/0D50X00009XkeGq/what-usarts-can-be-used-for-boot-on-64pin-stm32f401rct6-stm32f401xbc?t=1576434345679 was left unanswered. The words "The USART2 uses its remapped pins" in AN2606 gives the impression that non default pins can be used to access the bootloader. Is this the case? If so, how is it done?

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
bassetteporn11
Associate II

Thats a great question.

I actually wondered the same when I was designing my SPI bootloader pinouts on SPI4, I added a series on transmit pin of the chip that is being booted, since it cant have its slew rate controlled and default value is unknown to me, since it was 82mm it could cause reflection if slew is very fast I figured ok I'll be extra careful and plan for the worst.

I also said to myself NOOOO remapping.

I think the answer was you can't use USART2 PA2/PA3, perhaps you don't like the answer, but it was one.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User

I guess the expression "remapped pins" comes as a relic from the 'F1's GPIO/AFIO architecture. It probably shouldn't be formulated in that way for any other family.

IMO AN2606 is quite clear in describing which pins are used for the factory bootloader.

JW

I like your haircut, is that you?

You look like a badass.

CR.11
Associate

Thanks for the quick responses. The wording did provide a glimmer of hope but I did suspect that it wasn't possible. With regards to whether its clear enough. Clearly not. I'm not the first person to ask this question. Its quite an important limitation. Cube IDE makes it very easy to choose pins that would work fine in application code but not with the bootloader. It does this automatically if you have happened to have already used them for something else. If I were writing AN2606 I would certainly clarify that all USART bootloaders support default pins only and remove the "remapped pins" line if it no longer applies.

bassetteporn11
Associate II

Yeah well, as a self taught programmer with not much experience I wondered to myself, how can the micro know what its supposed to do in an absolute vacuum of information after a reset or in its default config?

That documents makes it even more obvious.