cancel
Showing results for 
Search instead for 
Did you mean: 

Can the ROM bootloader in the STM32H7 be configured to use the high speed USB interface instead of the full speed USB interface?

chriscole
Associate III
 
1 REPLY 1

It can do only what's indicated in the AN2606 app note.

The high-speed modes typically use an external PHY, adding to the complexity.

Generally the ROM is designed to handle a sub-set of functionality to provide a limp-home type recovery mode/method that's only dependent on what's within the chip, and not dependent on external circuitry and board level complexity.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..