2020-09-14 2:04 AM
Hello
I'm using the USB CDC class on my STM32H7.
Currently, I am using ST's VID (0x0483) and PID (0x5740).
I have four questions.
1.Can I use ST's VID and PID in our final product version?
2.If so, can I redistribute ST's Virtual COM Port driver to our customers?
3.How much does it cost to use ST's VID (0x0483) and unique PID?
4.We have a USB VID, but how much does it cost to change the VCP driver if we use our VID?
Best Regards,
2020-09-14 5:01 AM
You don't need a "VCP driver". Any decent OS supports CDC compatible devices in-box these days. Just make sure your device works well with these in-box drivers.
-- pa
2020-09-14 5:35 PM
Dear Pavel A,
Thank you for your quick reply.
At first I thought so too.
However, it seems that a VCP driver is needed for Windows 7 and Windows 8.1.
Actualiy, it didn't work on my Windows 7 PC without the VCP driver.
Best Regards,