cancel
Showing results for 
Search instead for 
Did you mean: 

Can anyone suggest how to work with both SD card and USB Thumb/flash drive with NUCLEO-H743ZI2 board in a single code?

Ssama.2
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee

Hi @Ssama.2​ ,

Is your request to have multidrives (USB Disk, uSD) configuration?

If yes, this is exactly what offers the example STM32Cube_FW_H7\Projects\STM32H743I-EVAL\Applications\FatFs\FatFs_MultiDrives.

STM32H743I-EVAL is based on the same device as NUCLEO-H743ZI2.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.