2024-08-02 12:52 AM
I'm trying to port over a JUCE framework project (a wavetable VCO), and I'd like to test it on a Nucleo-F446RE that I got about a year ago.
My entire build system is a clone of this lady Emilie Gillet's code base that she used to build eurorack modules. It's not quite HAL, and I guess not quite Bare Metal, but somewhere in between?
My repository is here.
https://github.com/eclewlow/eurorack/tree/master/waves2
I'm just porting over a little bit of code at a time. One thing I ran into was virtual functions being called just causing the flow of execution to stop. I don't think it's a hard fault, but the execution of the MCU definitely stops.
For example, in bootloader.cc
https://github.com/eclewlow/eurorack/blob/master/waves2/bootloader/bootloader.cc
void Init() {
System sys;
sys.Init(false);
sys.StartTimers();
GPIO_ResetBits(GPIOA, GPIO_Pin_5);
BufferAllocator allocator(shared_buffer, 16384);
childA.Paint();
Engine* e = &childA;
volatile size_t counter = 1000000;
while (counter--);
e->Paint(); // the execution reaches here and then stops, and the LED does not blink
GPIO_SetBits(GPIOA, GPIO_Pin_5);
}
int main(void) {
Init();
// after Init calls, infinitely blink once per second
// If I call the virtual function e->Paint() in Init(), then
// this following code will never execute.
while (1) {
if((system_clock.milliseconds() / 1000) % 2 < 1) {
GPIO_SetBits(GPIOA, GPIO_Pin_5);
} else {
GPIO_ResetBits(GPIOA, GPIO_Pin_5);
}
}
}I'm a newb to compilers and linkers, so if there is an error there, I would have no idea.
I've been messing around with compiler and linker flags, and the linker script.
One thing I noticed was at first the vtable entries in the .map file were missing? And it wasn't until I edited the linker script file did the vtables show up. However, it didn't fix the issue.
https://github.com/eclewlow/stmlib/commit/c1e4fb1913e813cdc76abfb34ccc4ab5793ce8a3
https://github.com/eclewlow/stmlib/blob/master/linker_scripts/stm32f4xx_flash.ld
The .map file seems to show a vtable entry for each virtual function, and they are assigned to different spaces in memory. Are the memory addresses somehow incorrect maybe?
*(.rodata)
*(.rodata*)
.rodata._ZTVN6waves26EngineE
0x0000000008000600 0x10 build/waves2_bootloader/bootloader.o
0x0000000008000600 vtable for waves2::Engine
.rodata._ZTVN6waves26ChildAE
0x0000000008000610 0x10 build/waves2_bootloader/child_a.o
0x0000000008000610 vtable for waves2::ChildA
.rodata._ZTVN6waves26ChildBE
0x0000000008000620 0x10 build/waves2_bootloader/child_b.o
0x0000000008000620 vtable for waves2::ChildBI'm building the code on a MacOS Sonoma 14.5, with the arm-4.8.3 release, as recommended by Emilie. Although, what's really recommended is building in a virtual machine, which I'm not doing.
2024-08-02 4:19 AM
When you debug the code and step through execution on that line, what happens?
2024-08-02 6:33 PM - edited 2024-08-02 6:34 PM
Thank you for your response.
So I don't know how to debug without CubeIDE, so I created a new CubeIDE project targeting my current Nucleo board.
There was no need to debug there. The code runs fine. The virtual function is called followed by blinking the LED.
I tried to dig around a little bit: checking out the makefile and linker scripts that are auto-generated by CubeIDE. They are different than the build system I was using.
I'll just use CubeIDE.