2017-06-13 12:14 AM
I'm using an STM32F103 and flashing a code into it using the bootloader. I'm successful in writing the code into the MCU, but when I try reading it using the Read Memory command (pg13) [
] it fails at step 6 (Send the number of bytes to be read (1 byte) & a checksum (1 byte).) I receive a NACK. It's confusing here, so I tried sending both XOR of 8th byte with 0 and in the next try tried sending complement of 8th byte, both failed.Here's what I'm doing:
1. Read 128 byte of the file to be written from SD card
2. Write this 128 bytes into the STM32 flash (code space) through the boot loader //works perfectly fine
3. Read back the recently written 128 bytes to verify if the write was successful.
4. If data written == read, move on. Write the next set of data.
5. Loop till the whole file has been written.
6. Send GO command and reset the STM.
P.S. I know the write command is working because previously I only had the write command, and it was working in the field. But some devices were flashed with the wrong/ corrupted code. So I'm reading back and checking if the data were written is the right one.
#stm32 #boot-loader2024-01-24 8:05 AM
@Clament John wrote:
Posted on June 13, 2017 at 09:14... but when I try reading it using the Read Memory command it fails at step 6 (Send the number of bytes to be read (1 byte) & a checksum (1 byte).) I receive a NACK. It's confusing here, so I tried sending both XOR of 8th byte with 0 and in the next try tried sending complement of 8th byte, both failed ...
#stm32 #boot-loader
Hi,
it is an old issue but I had the same problem. I think there is specification failure. Try to add +1 to calculate the check sum for the amount of data you want to receive. This solves the problem for me.
example you want to get 128 bytes: 0x7F (data), 0x7F (checksum) => NACK
correct: 0x7F (data), 0x80 (checksum) => OK
2024-01-24 10:13 AM
I'm not convinced.
Show an actual transactional example. I don't recall having issues with the AN3155 protocol docs and F1 parts, but the docs have likely been reworked a few times in the last 15+ years
2024-01-24 11:35 PM
What should I say. The current specification AN3155 doesn't work with a STMF103C8 for the Read Memory Command. It takes me one day to find a solution for this error.
AN3155
If you take Byte 8 (127) and make a XOR of Byte 8 (127) for Byte 9, you will get a NACK.
If you take Byte 8 (127) and make a XOR of Byte 8 +1 (128) for Byte 9, you will get an OK.
I found this solution by sniffing the communication of the old program "Flash Loader Demo".
But this is only for the Read Memory Command and there only for Byte 9!
2024-02-27 1:06 PM
I think I have figured this out as I was having the same issue. The key is the wording in AN3155:
"Checksum: XOR byte 8 (complement of byte 8)"
It actually means that the second byte is the complement of the first byte. In C, this would be the ~ operator. This is the same as the command byte.
Example 1:
Byte 0 = 0x01 (Read 2 bytes)
Byte 1 = 0xFE
Example 2:
Byte 0 = 0x7F (Read 128 byte)
Byte 1 = 0x80