Bootloader HardFault Error Peripheral
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-10 5:21 AM
Hi guys,
I'm using a bootloader. I am using 2 UART channels in the bootloader program. At the same time, I use these uart channels in the program I will install. But they don't work. The program enters the HardFault Error interrupt. When sending data to the uart channel when debugging, the program is corrupted and enters the HardFault Error interrupt.
What can I do?
Thanks..
- Labels:
-
Bootloader
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-11 6:18 AM
>>This general problem. But no enough information.
So have you looked at the registers and faulting instructions? Hard to debug remotely. Harder with no detail from the remote end, and selective cut-n-paste of code that may or may not be relevant to the failure.
In Keil the stack size is defined in startup_stm32f0xx.s
You need to make sure the app doesn't use the base of RAM you're using for the Vector Table, and that the RAM is remapped properly.
Make sure it is linking the correct library, 32-bit ARM libraries will not execute on a CM0, code built for the CM3 or CM4 will likely also fail.
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
‎2018-12-11 6:28 AM
Thank you for reply. This my .s file
; Amount of memory (in bytes) allocated for Stack
; Tailor this value to your application needs
; <h> Stack Configuration
; <o> Stack Size (in Bytes) <0x0-0xFFFFFFFF:8>
; </h>
Stack_Size EQU 0x400
AREA STACK, NOINIT, READWRITE, ALIGN=3
Stack_Mem SPACE Stack_Size
__initial_sp
; <h> Heap Configuration
; <o> Heap Size (in Bytes) <0x0-0xFFFFFFFF:8>
; </h>
Heap_Size EQU 0x200
AREA HEAP, NOINIT, READWRITE, ALIGN=3
__heap_base
Heap_Mem SPACE Heap_Size
__heap_limit
PRESERVE8
THUMB
; Vector Table Mapped to Address 0 at Reset
AREA RESET, DATA, READONLY
EXPORT __Vectors
EXPORT __Vectors_End
EXPORT __Vectors_Size
__Vectors DCD __initial_sp ; Top of Stack
DCD Reset_Handler ; Reset Handler
DCD NMI_Handler ; NMI Handler
DCD HardFault_Handler ; Hard Fault Handler
DCD 0 ; Reserved
DCD 0 ; Reserved
DCD 0 ; Reserved
DCD 0 ; Reserved
DCD 0 ; Reserved
DCD 0 ; Reserved
DCD 0 ; Reserved
DCD SVC_Handler ; SVCall Handler
DCD 0 ; Reserved
DCD 0 ; Reserved
DCD PendSV_Handler ; PendSV Handler
DCD SysTick_Handler ; SysTick Handler
; External Interrupts
DCD WWDG_IRQHandler ; Window Watchdog
DCD PVD_VDDIO2_IRQHandler ; PVD through EXTI Line detect
DCD RTC_IRQHandler ; RTC through EXTI Line
DCD FLASH_IRQHandler ; FLASH
DCD RCC_CRS_IRQHandler ; RCC and CRS
DCD EXTI0_1_IRQHandler ; EXTI Line 0 and 1
DCD EXTI2_3_IRQHandler ; EXTI Line 2 and 3
DCD EXTI4_15_IRQHandler ; EXTI Line 4 to 15
DCD TSC_IRQHandler ; TS
DCD DMA1_Channel1_IRQHandler ; DMA1 Channel 1
DCD DMA1_Channel2_3_IRQHandler ; DMA1 Channel 2 and Channel 3
DCD DMA1_Channel4_5_6_7_IRQHandler ; DMA1 Channel 4, Channel 5, Channel 6 and Channel 7
DCD ADC1_COMP_IRQHandler ; ADC1, COMP1 and COMP2
DCD TIM1_BRK_UP_TRG_COM_IRQHandler ; TIM1 Break, Update, Trigger and Commutation
DCD TIM1_CC_IRQHandler ; TIM1 Capture Compare
DCD TIM2_IRQHandler ; TIM2
DCD TIM3_IRQHandler ; TIM3
DCD TIM6_DAC_IRQHandler ; TIM6 and DAC
DCD TIM7_IRQHandler ; TIM7
DCD TIM14_IRQHandler ; TIM14
DCD TIM15_IRQHandler ; TIM15
DCD TIM16_IRQHandler ; TIM16
DCD TIM17_IRQHandler ; TIM17
DCD I2C1_IRQHandler ; I2C1
DCD I2C2_IRQHandler ; I2C2
DCD SPI1_IRQHandler ; SPI1
DCD SPI2_IRQHandler ; SPI2
DCD USART1_IRQHandler ; USART1
DCD USART2_IRQHandler ; USART2
DCD USART3_4_IRQHandler ; USART3 & USART4
DCD CEC_CAN_IRQHandler ; CEC and CAN
DCD USB_IRQHandler ; USB
__Vectors_End
__Vectors_Size EQU __Vectors_End - __Vectors
AREA |.text|, CODE, READONLY
; Reset handler routine
Reset_Handler PROC
EXPORT Reset_Handler [WEAK]
IMPORT __main
IMPORT SystemInit
LDR R0, =SystemInit
BLX R0
LDR R0, =__main
BX R0
ENDP
; Dummy Exception Handlers (infinite loops which can be modified)
NMI_Handler PROC
EXPORT NMI_Handler [WEAK]
B .
ENDP
HardFault_Handler\
PROC
EXPORT HardFault_Handler [WEAK]
B .
ENDP
SVC_Handler PROC
EXPORT SVC_Handler [WEAK]
B .
ENDP
PendSV_Handler PROC
EXPORT PendSV_Handler [WEAK]
B .
ENDP
SysTick_Handler PROC
EXPORT SysTick_Handler [WEAK]
B .
ENDP
Default_Handler PROC
EXPORT WWDG_IRQHandler [WEAK]
EXPORT PVD_VDDIO2_IRQHandler [WEAK]
EXPORT RTC_IRQHandler [WEAK]
EXPORT FLASH_IRQHandler [WEAK]
EXPORT RCC_CRS_IRQHandler [WEAK]
EXPORT EXTI0_1_IRQHandler [WEAK]
EXPORT EXTI2_3_IRQHandler [WEAK]
EXPORT EXTI4_15_IRQHandler [WEAK]
EXPORT TSC_IRQHandler [WEAK]
EXPORT DMA1_Channel1_IRQHandler [WEAK]
EXPORT DMA1_Channel2_3_IRQHandler [WEAK]
EXPORT DMA1_Channel4_5_6_7_IRQHandler [WEAK]
EXPORT ADC1_COMP_IRQHandler [WEAK]
EXPORT TIM1_BRK_UP_TRG_COM_IRQHandler [WEAK]
EXPORT TIM1_CC_IRQHandler [WEAK]
EXPORT TIM2_IRQHandler [WEAK]
EXPORT TIM3_IRQHandler [WEAK]
EXPORT TIM6_DAC_IRQHandler [WEAK]
EXPORT TIM7_IRQHandler [WEAK]
EXPORT TIM14_IRQHandler [WEAK]
EXPORT TIM15_IRQHandler [WEAK]
EXPORT TIM16_IRQHandler [WEAK]
EXPORT TIM17_IRQHandler [WEAK]
EXPORT I2C1_IRQHandler [WEAK]
EXPORT I2C2_IRQHandler [WEAK]
EXPORT SPI1_IRQHandler [WEAK]
EXPORT SPI2_IRQHandler [WEAK]
EXPORT USART1_IRQHandler [WEAK]
EXPORT USART2_IRQHandler [WEAK]
EXPORT USART3_4_IRQHandler [WEAK]
EXPORT CEC_CAN_IRQHandler [WEAK]
EXPORT USB_IRQHandler [WEAK]
WWDG_IRQHandler
PVD_VDDIO2_IRQHandler
RTC_IRQHandler
FLASH_IRQHandler
RCC_CRS_IRQHandler
EXTI0_1_IRQHandler
EXTI2_3_IRQHandler
EXTI4_15_IRQHandler
TSC_IRQHandler
DMA1_Channel1_IRQHandler
DMA1_Channel2_3_IRQHandler
DMA1_Channel4_5_6_7_IRQHandler
ADC1_COMP_IRQHandler
TIM1_BRK_UP_TRG_COM_IRQHandler
TIM1_CC_IRQHandler
TIM2_IRQHandler
TIM3_IRQHandler
TIM6_DAC_IRQHandler
TIM7_IRQHandler
TIM14_IRQHandler
TIM15_IRQHandler
TIM16_IRQHandler
TIM17_IRQHandler
I2C1_IRQHandler
I2C2_IRQHandler
SPI1_IRQHandler
SPI2_IRQHandler
USART1_IRQHandler
USART2_IRQHandler
USART3_4_IRQHandler
CEC_CAN_IRQHandler
USB_IRQHandler
B .
ENDP
ALIGN
;*******************************************************************************
; User Stack and Heap initialization
;*******************************************************************************
IF :DEF:__MICROLIB
EXPORT __initial_sp
EXPORT __heap_base
EXPORT __heap_limit
ELSE
IMPORT __use_two_region_memory
EXPORT __user_initial_stackheap
__user_initial_stackheap
LDR R0, = Heap_Mem
LDR R1, =(Stack_Mem + Stack_Size)
LDR R2, = (Heap_Mem + Heap_Size)
LDR R3, = Stack_Mem
BX LR
ALIGN
ENDIF
END
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-11 6:29 AM
I can't understand this file. Can you help me?
Thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-11 6:48 AM
>>Can you help me?
Does it pay well? I have a fence that needs stripping and repainting, can you help with that?
Stack_Size EQU 0x400 ; << make this more bigger
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
‎2018-12-11 7:30 AM
I am student man. If i work job i pay you. But now Can you pay me :)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-11 7:30 AM
I changed 0x800 but result not different. :(
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-11 11:15 PM
Any ideas? ​
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-11 11:37 PM
Did you mention the toolchain ? I can't remember.
The file you posted might get rewritten, better change the stack size in the project properties.
Try single-stepping in the debugger.
> can't understand this file. Can you help me?
Get someone tutoring you on site.
Doing this over such a forum will not work out, there is much for you to learn.

- « Previous
-
- 1
- 2
- Next »