2023-02-21 6:40 AM
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2023 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define ADDR_PROGRAM1 0x08003C00
#define ADDR_PROGRAM2 0x08033C00
/*
#define ADDR_PROGRAM1 0x3C00
#define ADDR_PROGRAM2 0x33C00
*/
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
#define MAJOR 0 /*version 0*/
#define MINOR 1 /*version 1*/
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
const uint8_t BL_Version[2]={MAJOR,MINOR};
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
/* USER CODE BEGIN PFP */
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void goto_application( void );
typedef void (*pFunction)(void);
pFunction Jump_To_Application;
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
void (*SysMemBootJump)(void);
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
/* USER CODE BEGIN 2 */
//HAL_RCC_DeInit();
//__disable_irq();
/*__HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH(); // nécessaire (réinitialise le system memory)? */
/************/
/*
SysMemBootJump = (void (*)(void)) (*((uint32_t *)(ADDR_PROGRAM2+4)));
__set_MSP(*(uint32_t *)ADDR_PROGRAM2); // Main Stack Pointer
SysMemBootJump();
*/
/************/
HAL_Delay(1000);
Led10_Flash(1);
HAL_Delay(3000);
goto_application();
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.MSICalibrationValue = 0;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_5;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(Led10_GPIO_Port, Led10_Pin, GPIO_PIN_SET);
/*Configure GPIO pin : Led10_Pin */
GPIO_InitStruct.Pin = Led10_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(Led10_GPIO_Port, &GPIO_InitStruct);
}
/* USER CODE BEGIN 4 */
void Led10_Flash(char Nombre)
{
char x1;
HAL_GPIO_WritePin(Led10_GPIO_Port, Led10_Pin, GPIO_PIN_RESET);
for (x1=0;x1<(Nombre*2);x1++)
{
HAL_GPIO_TogglePin (Led10_GPIO_Port, Led10_Pin);
HAL_Delay(500);
}
HAL_GPIO_WritePin(Led10_GPIO_Port, Led10_Pin, GPIO_PIN_RESET);
}
static void goto_application(void)
{
uint32_t JumpAddress;
JumpAddress = (uint32_t) *((__IO uint32_t*)ADDR_PROGRAM2);
Jump_To_Application = (pFunction) *(__IO uint32_t*) (ADDR_PROGRAM2 + 4);
SCB->VTOR = JumpAddress;
__set_MSP(JumpAddress);
Led10_Flash(5);
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
2023-02-21 6:48 AM
Code in SystemInit() tends to set SCB->VTOR
Check the build address in the linker script is correct.
Use a debugger, step the transition, understand what's "not working"
2023-02-21 7:29 AM
2023-02-21 7:30 AM
It's like if there was an uncompatilbility between two files from different compilers.
If I remove "SCB->VTOR" it doesn't change anything...
Is it possible, for example to add a short program in the STMCube "bootloader" soft (adress 0x08033C00) so I can test if it work and try to compare ? (hard to learn a new way of writing code...)
2023-02-22 6:02 AM
Nobody can answer ? is it really possible to jump to an application , made with other compiler, or did the
compilation made includes a specific area that would not allow it ?
I tried this too but it doesn't change anything (soft is "lost"):
#define ApplicationAddress 0x08033C00
typedef void (*pFunction)(void);
uint32_t JumpAddress = *(__IO uint32_t*) (ApplicationAddress + 4);
pFunction Jump_To_Boot = (pFunction) JumpAddress;
__set_MSP(*(__IO uint32_t*) ApplicationAddress);
Jump_To_Boot();