cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi support and/or best practice for new board-design?

Southbranch
Senior II

Hi!

I basically have two questions:

  • Regrettably, there are no STM32 MCU:s that comes with built in Wi-Fi support and I am curious to fund out the reason for this? Perhaps any new products in the pipe? The need for new IoT applications must by huge these days...

  • In the meanwhile, we have started up a custom board design based on a STM32H7. The board needs Wi-Fi and my question is if there are any "HW-best-practice" tips using a 3rd party Wi-Fi chip/modules? So far, we are thinking of using the Type 1DX| LBEE5KL1DX | Murata Manufacturing Co., Ltd which supports both WiFi + BLE. The dilemma is that drivers needs to be ported to the STM32 environment which would be cumbersome...

Any comments would be highly appreciated!

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
T J
Lead

these guys are not ST staff, but these guys can help you.

strip antenna... , that depends on the required range, 50-100M should be ok

you can do it in 2 layers, if you wanted the pcbs for 50c each..