cancel
Showing results for 
Search instead for 
Did you mean: 

Why am I getting only 1v from 3v3 when I unplug ST-LINK

KAsk.1
Associate

When developing I'm using the ST-LINK to transfer my code to the stm32. All is well when it is plugged in but I'm only getting 1v from the 3v3 pin when I disconnect and run from usb. 5v is still 5v.

I've connected an hx711 with a load cell and also a 2x16 lcd but the lcd shuts down when unplugging the ST-LINK.

Does this mean I need an external power supply or can I use the 5v to get the 3v3?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Ozone
Principal III

> Does this mean I need an external power supply or can I use the 5v to get the 3v3?

I suppose so.

Some while ago, I had the same problem with attached LCD display.

USB delivers up to 100mA to an attached sink. It can deliver up to 500mA if the device explicitly requests it - which your target device surely does not.

I assume you are using a Nucleo ar Discovery board, that has different power sources OR'ed via schottky diodes.

KAsk.1
Associate

I'm using the blue pill...

Would it be worth trying to add the 3v3 from 5v with a resistor?