cancel
Showing results for 
Search instead for 
Did you mean: 

What type of camera should i use with STM32F746G Discovery board?

Tajwar.Chandel
Associate III

Hi ST Team,

Please suggest an camera part number which i can easily interface with the 32F746GDISCOVERY Board. 

Kindly share the complete details.

 

Thanks & Regards,

1 ACCEPTED SOLUTION

Accepted Solutions

Hello again @Tajwar.Chandel 

You can connect the board to the camera module using the  1 × 30 pin ZIF connector of each one of them.

For the camera module :

Screenshot_2023-12-16-17-22-28-02_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

For the board :

Screenshot_2023-12-16-17-22-46-58_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

for more details, refer to the UM1907 and the UM2779.

Best Regards. 

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
STTwo-32
ST Employee

Hello @Tajwar.Chandel 

You can use the B-CAMS-OMV camera module that is compatible with the STM32F4DIS-CAM camera module, so you can connect it to your STM32F746 Discovery board. The drivers of the B-CAMS-OMV can be found in the AI vision function pack.

 

Best Regards,

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Tajwar.Chandel
Associate III

Hi,

Can you please share any  document for how to connect (interface) the  B-CAMS-OMV camera module with 32F746GDISCOVERY Board. Hope you will help.

Regards,

Tajwar

Tajwar.Chandel
Associate III

Hi,

Can you please share any  document for how to connect (interface) the  B-CAMS-OMV camera module with 32F746GDISCOVERY Board. Hope you will help.

 

Regards,

Tajwar

Hello again @Tajwar.Chandel 

You can connect the board to the camera module using the  1 × 30 pin ZIF connector of each one of them.

For the camera module :

Screenshot_2023-12-16-17-22-28-02_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

For the board :

Screenshot_2023-12-16-17-22-46-58_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

for more details, refer to the UM1907 and the UM2779.

Best Regards. 

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello,

Please provide link to sample project for interfacing the 32F746GDISCOVERY - Discovery kit with camera module B-CAMS-OMV.

 

Regards,

Tajwar