2019-04-29 03:19 AM
what's the meaning of the "SN",readed from "STM32 ST-link Utility"
I read the UID from the Flash addr 0x1FFFF7E8, i found out the SN
is not the UID. please tell me where is the SN 'data from? tks
Solved! Go to Solution.
2019-04-29 04:11 AM
As it says: It is the serial number of the STLink. You target has another serial number.
2019-04-29 04:11 AM
As it says: It is the serial number of the STLink. You target has another serial number.
2019-04-29 04:15 AM
wow, Thank you very much!
2019-04-30 01:50 PM
@Uwe Bonnes Where can we read the serial number from? IS there a memory location, where is it documented?
2019-04-30 02:45 PM
The ST's serial number, or the UNIQUE ID of the part you're running? The Reference Manual, or Data Manual, should provide the address where the UNIQUE ID is situated.