cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743ZI2 NUCLEO board Ethernet doesn't work when moving to JP5 to 1.8V (MCU_VDD)

DGany.2
Associate II

Hi All,

I use the STM32H743ZI2-NUCLEO board with JP5 on 1.8V for MCU_VDD.

Running the LWIP example, the Ethernet doesn't work (It does work when running with 3.3V).

Any idea how to make it work with 1.8V?

Thanks,

David

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
KDJEM.1
ST Employee

Hello @Community member​,

Please make sure that  R4, R43, R44, R45, R46, R47, R48, R49, R50, R51, R52, R53, R59, R61, U1, U10, U15, and SB45 are not removed.

Because after removing these components, it becomes impossible to use Ethernet with1.8 V.

For more explanation, I advise you to refer at the UM2407.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

DGany.2
Associate II

Hi Kaouthar,

Thanks for your reply.

The board is at its manufacturing state, no component was removed.

I just moved JP5 to 1.8V and the ETHERNET stopped working.

Any idea why?

Thanks,

David