2025-09-23 10:47 PM
Hi,
Can you please confirm if the STM32H743I-EVAL board can be used to evaluate the STM32H743VIT6 IC?
While checking the documentation, I noticed that the evaluation board shows NRND status with the STM32H743XI.
2025-09-24 12:52 AM - edited 2025-09-24 12:52 AM
In fact, the STM32H743I-EVAL is already on NRND, but this is not a major problem because the STM32H753I-EVAL can be used instead. It is identical to the STM32H743I-EVAL except for the STM32H743XI providing an additional AES encryption hardware unit. If you do not use this AES unit, the board behaves identically to the other one.
You can use both EVAL boards to evaluate the STM32H743VI, but you should bear in mind that the STM32H743XI has 240 pins and the STM32H743VI only has 100 pins. In addition, the STM32H743VI has a minimum VCC of 1.71V, while the STM32H743XI is guaranteed to work down to 1.62V. Due to the smaller package, fewer functions are available externally on the STM32H743VI (fewer GPIOs, fewer tamper and wake-up pins, fewer ADC channels).
Hope that helps?
Regards
/Peter