cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746GDISCOVERY code example for DCMI

Hephaestus
Associate

Does anyone know where to find a code example for using DCMI on STM32F746G-DISCO? AN5020 says there are 5 examples based on STMCubeMX  (section 8.3 p53). But, I can't find any examples for this when I try using STMCubeMX. It doesn't matter which SELECTOR I try.

Nor can I find a code example for this when I use "Import STM32Cube example" in STMCubeIDE.

Thanks,

 

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STTwo-32
ST Employee

Hello @Hephaestus and welcome to the ST Community :smiling_face_with_smiling_eyes:.

You can implement all 5 projects following the detailed description on the pages 54 to 73 of the AN5020.

PS: capture of JPEG data is implemented using the STM324x9I-EVAL and OV2640 CMOS sensor.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.