2025-04-24 3:40 AM
We are making a FCU based on STEVAL-FCU001V2 as a study project. We have manufactured the pcb from the gerber files that ST provided. We have had the components stuffed on the pcb as well. We uploaded the ST firmware provided by ST in our drone from this link: "https://www.st.com/en/embedded-software/stsw-fcu001.html", Specifically The STEVAL-FCU001V1 program using the ST-Link V2. We uploaded this code as this is the only code that was built without any errors in the cubeide. Now we know that the code is uploaded inside the board as when we press reset button, the onboard led turns on. But in the STDrone App, we cannot see the drone. The BLE sensor used is the BlueNRG-M0A. It is working as well as by using multimeter we measured the power consumption between its VDD and GND pin to be 3.3 volts. The define statement in the code is also set to "#define REMOCON_BLE // BLE Remocon App" but still we cannot see the drone in the app.
Any help would be appreciated. Thank you for your time.