2025-12-28 5:11 AM - last edited on 2025-12-28 6:19 AM by mƎALLEm
Hi All,
I'm building an instrument that needs to stream data to a PC at ~4Mbps. People were claiming nearly twice this with USB CDC so I chose the nucleo-h533 board and started with the Ux_Device_CDC_ACM example. I disconnected the USART code and added a loop that calls ux_device_class_cdc_acm_write and then I measure the rate at which I receive data on the PC. I can't get past ~1.8Mbps.
I have tried the following:
In all cases, the baud rate remains about the same at 1.8Mbps. Is there anything I can do to improve this?
Best,
Marc
2025-12-28 8:19 AM
The PC side needs to poll quickly enough. Most programs do not do this. What are you using on the PC side? Eliminate hubs from the chain. Ensure you send a new buffer immediately after the previous buffer is sent.