2025-07-01 9:26 AM - last edited on 2025-07-01 9:46 AM by Andrew Neil
Dear all,
I would be interested to use a MKI109D dev board (with USB C connector) to stream data from a MKI178V2 board fitted with a SM6DSL IMU sensor to a preferably a python or cpp based script using something like a pyserial library. I have tested the board and the IMU with the MEMS Studio software and flashed it with the correct firmware , and therefore can see the IMU output as intended. However when trying to connect to the dev board using pyserial, after opening the COM port , and transmitting the *dev command, I receive an error that the device is not supported. I would appreciate some help on some direction as to what the problem here might be and if possible a minimal set of python (or cpp) command to read out the IMU data.
Many thanks in adveance.
2025-07-02 2:30 PM
Hi @SaeidD
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy