cancel
Showing results for 
Search instead for 
Did you mean: 

Interfacing issue

JanhaviDeshpande
Associate

Help needed on interfacing buzzer with L476

4 REPLIES 4
Peter BENSCH
ST Employee

Welcome @JanhaviDeshpande, to the community!

Many details are still missing:

  • buzzer data sheet (link to the data sheet would be fine)
  • what supply voltage will the buzzer have
  • what frequencies should the buzzer emit and at what volume?
  • which waveforms should be sent to the buzzer?
  • are you planning to use an amplifier stage, if so, which one (or do you need proposals)?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

First of all, Thankyou Sir for replying to the message.

Basically, using TMB12A05 active buzzer for a project based on anamoly detection based on audio. Basic functioning includes giving alert. 


@JanhaviDeshpande wrote:

First of all, Thankyou Sir for replying to the message.

Basically, using TMB12A05 active buzzer for a project based on anamoly detection based on audio. Basic functioning includes giving alert. 


Still not enough information on what you're trying to achieve.

  • "based on audio" - So do you have something that detects this audio? Microphone? Describe what this anomaly consists of.
  • The buzzer has a frequency range of 2300+/-300H. You need to have some kind of driver for it as well, which you haven't provided any schematic.
If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source


@JanhaviDeshpande wrote:

TMB12A05 active buzzer  


What's that?

As @Peter BENSCH said, give a link to its datasheet.

Please see the posting guidance on how get good replies to your questions:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 

How To Interface Anything to Anything Else: http://www.8052mcu.com/forum/read/160143

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.