2024-08-16 7:46 AM
I'm using nucleof446reboard and I'm running out of digital pins. Is there a way to use analog pin as a digital pin??
Solved! Go to Solution.
2024-08-16 8:36 AM
Sure, just try. And see on circuit of the board, if the pins are free or connected to something.
I don't have the circuit here to see, so look yourself... :)
2024-08-16 8:13 AM - edited 2024-08-16 8:20 AM
All standard pins can be used digital, just see in Cube, what the pins can be set to - then you know.
And if a pin already set to analog, Set it to unused, then you can choose, what ever is possible on this pin.
2024-08-16 8:29 AM
I have never changed the pins first set on the board separately. The analog pins I mentioned are the pins on the left side of the board. Can I change these pins from cube mx to digital pins?
2024-08-16 8:36 AM
Sure, just try. And see on circuit of the board, if the pins are free or connected to something.
I don't have the circuit here to see, so look yourself... :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.