cancel
Showing results for 
Search instead for 
Did you mean: 

How to connect VREF+ pin on stm32F722RET6?

VKoga.1
Associate II

I am designing a custom PCB using STM32F722RET6. How to connect the VREF+ pin(13) on the SMT32F722RET6?.

As per the hardware development manual, it says

"The VREF+ pin can be connected to the VDDA external power supply"

and then, "VDDA=VDD and VSSA=VSS."

can I connect it to 3.3V external supply?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @VKoga.1​, to the community!

yes, you can connect it to VDD. Please also read the General PCB Design Guidelines with figure 51 in the datasheet.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @VKoga.1​, to the community!

yes, you can connect it to VDD. Please also read the General PCB Design Guidelines with figure 51 in the datasheet.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
VKoga.1
Associate II

Thank you so much, like always never been let down by ST.