Skip to main content
SCook.1
Associate III
Sep 10, 2021 9:25 AM UTC
Solved

Is it ok to connect an ST-LINK V2 to a board which has a powered 3.3V rail?

I ask because I need to test the analogue part of a (custom) board which is powered from 12V, but also generates a 3.3V rail from that. I'd prefer to leave the ST-LINK connected if at all possible.

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Sep 10, 2021 9:27 AM UTC

Yes, you can do that.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Sep 10, 2021 9:27 AM UTC

Yes, you can do that.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SCook.1
SCook.1Author
Associate III
Sep 11, 2021 7:43 AM UTC

I can confirm that it works. Thank you Peter.