2026-05-14 7:04 AM
Hi! I’m working with the STM32N6570-DK board using an object detection AI model, and I would like to manually modify the camera parameters. I believe settings such as exposure, white balance, and similar controls are currently configured automatically, but I want to use fixed/manual values instead.
I already tried modifying the cmw_camera.c file, but nothing changed. Which files do I actually need to modify in order to set specific camera parameter values? Do I need to use a dedicated tool for this?
I’m using the IMX335 camera module.