2020-11-27 7:30 AM
I have custom board with minimal design only stm32 chip is there and couple necessary capacitors and due to some soldering issue, i got shorted with 3.3 and gnd .. accidentaly i powered it on and for debuging it was connected like this for 2 minutes. now stm32 is not communicating through swd. Did it brick stm32 by shorting 3.3 and gnd for a minute ?
2020-11-27 9:44 AM
oh ok so my dot has to be straight instead of the text right ? can you please correct me if i am wrong since i only have one chip left and then i will have to order it and in my country it will come after a month
2020-11-27 9:55 AM
Now is it correct ? the dot is now in upper corner
2020-11-27 10:15 AM
2020-11-27 10:16 AM
Can you please elaborate ? I have updated the image with newer pcb and solder paste is attached just ready to solder after i have a confirmation that orientation is correct. Waiting for your confirmation
Thank you sir!!!
2020-11-27 4:57 PM
This orientation is now correct.
> Can you please elaborate ?
What I meant was I don't know how to interpret "oh ok so my dot has to be straight instead of the text right ?"
How can a dot be straight and text be right? How can you make a dot not straight? Maybe there is a second language problem at play here.
In any case, orientation is now correct based on the position of the crystal.
2020-11-28 1:41 AM
Hello Thank you sir for the help now it is working......